Part Number: TPS552882-Q1
Other Parts Discussed in Thread: TPS552892-Q1
We are using TPS552882-Q1 as a buck-boost regulator to generate 13.6V with 3A load current.
During testing, we are observing a random VOUT (VCC_PAVDD) failure. In the failed condition:
-
VOUT collapses to 0 V
-
On probing the device, the internal MOSFET appears to be shorted (VOUT, SW2 pins are shorted)
-
No external components (inductor, capacitors, resistors, MOSFETs) are found damaged or shorted.
-
Failure is intermittent and does not occur consistently.
We have tested the design with:
-
Continuous 3 A load current
-
Repetitive load change from 1 A to 3 A every 100 ms
During these tests, no abnormal behavior was observed.
We have attached the schematic and layout images. Kindly let us know if there are any concerns in the design that could cause and provide feedbacks to avoid this failure.