This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2116: TPS2116: PR1 voltage reference characteristic curve

Part Number: TPS2116

Hello,

Regarding the PR1 voltage reference on TPS2116DRLR, is there a characteristic curve that shows its behaviour over temperature?

image.png

Regards

Martin

  • Hi,

    Thanks for reaching out,

    There is no specific characteristic curve available for the PR1 voltage reference (VREF) temperature behavior in the TPS2116DRLR datasheet.

    But here the voltage ref characteristic curve is generally linear & predictable, at 27°C  Vref is 1V & it changes by + - 0.1%/°C when you go up & down respectively. 

    Thanks,

    Hemanth.