Part Number: TPS61094
The TPS61094 can discharge a supercapacitor to as low as 0.6V. However, hybrid supercapacitors have a minimum operating threshold—typically 2.2V or 2.5V—below which they should not be operated. Is it possible to adjust the TPS61094's (or another device?) discharge threshold, or is there a way to implement a circuit that shuts down the device once the supercapacitor voltage drops below 2.2V?
Thank you!