This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3410-Q1: Inquiry regarding device recommendations

Guru 12110 points

Part Number: LM3410-Q1
Other Parts Discussed in Thread: LM3410, , TPS61165-Q1

Hello,

My customer is looking for an LED driver IC that can support the following conditions:

- Number of LEDs: 9
- LED Connection Configuration: Series (1x9)   --> 3 x 3
- LED Color: White
- LED Driver IC Power: AAA Batteries (x2)
- LED Control: PWM
- LED : EVERLIGHT XI3030 Series
- Requirements:
   * AEC-Q100
   * Low Input Voltage (Below 2V is best, but in the early 2-volt range it is possible)
   * Output Voltage (35V or higher)
   * FB Voltage: 100mV (lower is preferred)

Please recommend the most suitable device among TI products.

Thank you.

  • Hi JH,

    What's your application? and what's your current requirement? Thanks!

  • Hello Hailee Xu,

    Thank you for your reply.

    The customer's target is a remote control for automotive applications.

    The LED characteristics are as follows:

    Regards,

    JH

  • HI JH,

    The main challenge for LM3410 is Vout range. do you want to have an auto-version device or non-auto is acceptable? or could you increase the input voltage? or is it possible to add a boost CV stage before the LED driver IC?

    May I know a specific scenario for "a remote control for automotive applications? Please let me know if you want to have a detailed discussion via the email. Thanks!

  • Hi Hailee Xu,

    Below is the customer's response.

    The target application is a BT remote control for a car rear seat monitor.

    Since we plan to use 2 battery cells (1.5V * 2 = 3V), the Vin(min) value in the specifications of LM3410-Q1 should be lower than the the early 2-volt range.

    For example, we thought a product like the Microchip MCP1664 would be appropriate. If you know of a TI alternative that's more efficient than the Microchip MCP1664, please let us know.

    Additionally, the LED connection configuration will use 3x3.

    Thanks!

  • Hi JH,

    Thanks for the update, regarding the LED connection configuration, do you mean 3p3s - three LEDs in series per string and three strings are connected?

    • if so, like I mentioned before, the challenge for LM3410-Q1 is about the Vout range, if the Vout could be close to 3 x VF, LM3410-Q1 could support it since the output voltage is within 24V. 
    • If not and considering the Vout of 35V, TPS61165-Q1 can be considered. Additionally, if you require a lower input voltage below 2V, we are developing a new device that perfectly meets your needs. if you are interested, we can discuss more details via the email.

    The above discussion is based on single-channel solution, please let me know if you require a three-channel solution. Thanks!

  • Hi Hailee,

    Thank you for your help.

    Here is the customer's response.

    Thanks for the update, regarding the LED connection configuration, do you mean 3p3s - three LEDs in series per string and three strings are connected?

    Correct.

    For LM3410-Q1, the VIN (min) specification is 2.7V, which is higher than the required specification and cannot be used.

    Please recommend another replacement that meets the specifications below.

    - AEC-Q100 Grade Compliant (Auto-Grade)
    - Low Input Voltage (Early 2V Range)
    - Output Current Limit (min) (200mA or more)
    - Output Voltage (20V or more)

    Please send me an email regarding new devices.

    Thanks!

  • Hi Hailee,

    The customer is waiting for your response. Thanks!

  • Hi JH,

    I will contact you via email. Thanks!