This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM365R1: Maximum output voltage unclear from datasheet

Part Number: TPSM365R1

Hi, 

I want to use TPSM365R1 or TPSM365R15 for voltage conversion from 24V to 16V. Datasheet (SNVSCI1A) gives Vout 16V for both Absolute Maximum Rating and Recommended Operating Condition. Problem is that if I use 1% feedback resistors (150k, 10k) output voltage will be at max. 16.3V, not taking into account feedback voltage tolerance. So Vout will probably be beyond the allowed maximum rating.

Is it save to use the device under that conditions?

Thank you very much in advance for clarification.