TPS4HC120-Q1: power up sequence

Part Number: TPS4HC120-Q1

Hi team,

 

Is there a problem if 3.3 V is applied to the /FLT terminal and the LPM terminal before the voltage is applied to VBB? The power supply pulls up at 10k PU comes up before VBB. ->

is there a risk of wrong operatin, latch-up, IC damage, etc.?

Also, is there a problem if the SEL0/1, DIAG_EN, and ILIM terminals EN1/2/3/4 are applied before VBB? " 

Best,

Shoo

  • Hi Shoo,

    As long as you are operating within the absolute max specs in the data sheet the device should not be damaged from operation, I would recommend putting the appropriate sized protection resistors to protect the device but other than that no damage should occur if it is applied before VBB is high

    Best Regards,
    Nicholas Petersilge