Part Number: TPS65219
Our customer wants to configure the EN/PB/VSENSE pin as "Device Enable" instead of "Push Button" to trigger the power-down-sequence using the logic output of another device.
Can the EN_PB_VSENSE_CONFIG field in the MFP_2_CONFIG register be changed from the default (NVM configuration)?
In the datasheet, it appears that the EN_PB_VSENSE_CONFIG field in the MFP_2_CONFIG register cannot be changed from the default (Push Button Configuration).
"Enable / Push-Button / VSENSE Configuration. Do not change via I2C after NVM load (except as a precursor before programming NVM) (Default from NVM memory)"
How to trigger the power‑down sequence using the logic output of another device?
Best regards,
Daisuke