Part Number: LM25116EVAL
Other Parts Discussed in Thread: LM25116
We have a design based on the LM25116 trying to generate 24Vout @ 10A from an 8S1P LiIon battery pack (25V-33.6V). the initial design was approached through the WebBench design tool which supplied a design that wasn't close to working. The spreadsheet tool downloaded (SNVU051) seemed to have better insight on the nuances and drawbacks of our initial design specs. Using the spreadsheet we attempted to reconfigure our board for a 15V output - but the output only gets to about 8.5 Volts.
We puchased the LM25116 EVAL board which is designed for 5V @ 7A and tried to reconfigure the output to 15V, but that too, only reaches 8.7V. We are trying to figure out: what is wrong with the calculations and what are we missing?
Attached are the spreadsheet and a snip of the parts changed on the eval board to try to reconfigure it to 15V out.
With regard to the original task of getting 24V @ 10A from the 8S1P lithium battery do you have a suggestion for a different design path?