This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25756E: Schematic Review Request - 140W USB-PD 3.1 Charger for 6S Li-ion

Part Number: BQ25756E
Other Parts Discussed in Thread: BQ25756, TPS26750, TPD4S480, TPS25751, TPD4S201, TPS25751EVM

We are designing a high-performance battery pack. We are using the BQ25756E to implement a 140W Bidirectional USB-PD 3.1 charging interface.

I would appreciate a review of my schematic and design calculator, specifically regarding component selection for 140W operation.

System Specifications:

Application: Portable Power Bank with 6x 21700 Cells.

Battery Config: 6S Li-ion (Standard NMC).

Battery Voltage: 16.0V (Min) – 25.2V (Max).

Input/Output: USB-PD 3.1 EPR (5V, 9V, 15V, 20V, 28V).

Target Power: 140W (28V @ 5A).

Inductor: 3.3microH (Saturation Current > 15A).

Sense Resistors: 2mohm (Input RAC), 5m (Battery RBAT).

Design Methodology & Questions: I have attached my schematic and the design calculator. Please note a specific configuration regarding the Input Voltage settings:

The "Hybrid" Calculator Setting: In the design calculator, I set VAC(min) to 20V (Row 5) but set ACUV to 4.2V (Row 58).

Reasoning: I want to support standard 5V USB charging (at low power), but I only require the full 140W capability when connected to a 20V+ EPR source. Setting VAC(min) to 5V in the tool resulted in unrealistic inductor sizing (~10microH+) for 140W.

Question: Is this "Hybrid" approach safe? Will the BQ25756 stability/compensation loop handle the transition from 5V (low power) to 28V (high power) with the 3.3microH inductor selected for the higher voltage range?

Inductor Selection (3.3microH): The calculator flags 3.3microH as close to the minimum. Given the wide input range (5V–28V) and wide battery range (16V–25.2V), is 3.3microH the optimal trade-off for a 140W target, or should I move to 4.7microH to reduce ripple at the expense of transient response?

Thermistor Placement: I have placed a 10k NTC thermistor physically adjacent to the main switching FETs (Q19-Q22) to throttle current if the power stage overheats. Does the BQ25756 handle thermal throttling autonomously via the TS pin, or does this require MCU intervention?

Finally, overall is my schematic ready to move into the PCB layout phase with component selection, which MOSFETS would you reccomend here?

Schematic and Calculator attached.

V1Charger.pdf 

BQ25756_DESIGN-CALC-V01X3.xlsx 

Thank you for your time and guidance.

  • Hello Merri,

    Have you reviewed your schematic with the schematic and layout checklist, yet?

    We also have an app note to help MOSFET selection, a reference design for 100W USB-PD charging, and 240W USB-PD charging.

    Does the BQ25756 handle thermal throttling autonomously via the TS pin, or does this require MCU intervention?

    This is automatic. The BQ25756 will follow the JEITA profile when the thermistor gets hot.

    Is this "Hybrid" approach safe? Will the BQ25756 stability/compensation loop handle the transition from 5V (low power) to 28V (high power) with the 3.3microH inductor selected for the higher voltage range?

    Yes, this is safe. Make sure to select the right switching frequency for the inductor. What is the switching frequency for your system?

    The calculator flags 3.3microH as close to the minimum. Given the wide input range (5V–28V) and wide battery range (16V–25.2V), is 3.3microH the optimal trade-off for a 140W target, or should I move to 4.7microH to reduce ripple at the expense of transient response?

    The 3.3µH and 4.7µH will both work good for the transient response. The main tradeoff between the 2 inductors will be the efficiency. Does your application have a size limit for the inductor.

    Let me know if you have reviewed the schematic with the checklist. Once you have gone through the checklist, I can do a final schematic review on my side.

    Best Regards,
    Ethan Galloway

  • Hi Ethan,

    Thank you for the guidance. I have reviewed the Schematic and Layout Checklist against my design and updated the schematic accordingly. I am holding off on starting the PCB Layout until you give the schematic a final green light.

    Design Updates:

    Inductor & Frequency: Moved to 4.7µH and lowered switching frequency to 400kHz (R_FSW = 66.67kΩ (should be correct)) to prioritize thermal efficiency in our enclosed form factor.

    Thermistor: Configured the JEITA network (RT1 = 5.23kΩ, RT2 = 30.1kΩ) for a standard 103AT NTC.

    Two Clarifying Questions:

    The CE (Charge Enable) Pin: The checklist implies this should be driven or pulled High, but since CE is Active Low, I have placed a 10kΩ Pull-Down resistor to GND.

    Reasoning: I want the default state to be "Charging Enabled" so the device can recover from a dead battery even if the MCU has no power to drive the pin.

    Question: Is this safe/recommended, or should I add a hardware delay?

    MCU Connections: The current schematic page focuses on the BQ25756 power stage. Do you need to see the MCU page to review how I am handling the I2C lines (SDA/SCL) and status signals (STAT/PG)? I want to ensure the logic levels and pull-ups match your expectations.

    Also since I am fairly new to power hardware can you explain the reasoning for the multiple decoupling capacitors in the reference designs (which I copied). 

    Finally will your review also cover the USB controller and the rest of the implementation?

    I have attached the updated Schematic (Rev 1.2) for your review.Rev1_2.pdf

    Best

    MJ

  • Hello Merri,

    Reasoning: I want the default state to be "Charging Enabled" so the device can recover from a dead battery even if the MCU has no power to drive the pin.

    Question: Is this safe/recommended, or should I add a hardware delay?

    Yes, this is safe.

    MCU Connections: The current schematic page focuses on the BQ25756 power stage. Do you need to see the MCU page to review how I am handling the I2C lines (SDA/SCL) and status signals (STAT/PG)? I want to ensure the logic levels and pull-ups match your expectations.

    These connections look good.

    Also since I am fairly new to power hardware can you explain the reasoning for the multiple decoupling capacitors in the reference designs (which I copied). 

    There are multiple reasons to have multiple different decoupling capacitors;

    • Multiple capacitors can have a lower ESR in parallel
    • Multiple capacitors are more resilient if one capacitor fails.
    • Multiple capacitors are shorter and can be easier to fit on a board compared to one big capacitor

    You might have already seen this, but we have an app note for the capacitors.

    Finally will your review also cover the USB controller and the rest of the implementation?

    I've looped in the USB controller team to review this portion.

    Your schematic looks good. I have 3 thoughts:

    • It looks like you have about 260uF on the input and the output. This will work for the BQ25756E, but you might be able to save money and board space by only using 160uF.

    • Make sure the VAC pins are shorted together close to the BQ25756.

    • I would also recommend adding a DNP 0 Ohm resistor to short DRV_SUP to REGN. This resistor will help with debugging.

    Best Regards,
    Ethan Galloway

  • Hello,

    Please find the attached.

    /cfs-file/__key/communityserver-discussions-components-files/196/SchChklist2p2a_5F00_01_5F00_21_5F00_2026.xlsx

    (1) Liquid detection is not supported on the TPS26750

    (2) You may want to connect the TPD4S480 to the LDO_3V3 of the TPS26750 to support dead battery operation.  This will depend upon the availability of the MCU_3V3 and what you desire to pass to the system in dead battery.  

    Regards,
    Chris

  • Thank you Ethan.

    The app note on capacitors is not showing up as existing when I click that link. I will add a 0 ohm resistor to short DRV_SUP to REGN. Are there any places that you see where I can save costs without compromising functionality? This is crucial or even removing parts as a whole would be great.

  • Ideally when plugged in I would like the mcu to be able to power up so how would we support this, would it be (2) that you mentioned?

    Additionally I read that pin for pin the TPS25751 is exactly identical drop in replacement for the TPS26750 so should I just use that instead? Appreciate all the feedback and guidance thus far.

  • Hello,

    Ideally when plugged in I would like the mcu to be able to power up so how would we support this, would it be (2) that you mentioned?

    I would recommend connecting the TPD device to LDO_3V3 to ensure that the PD can negotiate to the desired sink voltage to charge/power the system when the battery is dead. 

    Additionally I read that pin for pin the TPS25751 is exactly identical drop in replacement for the TPS26750 so should I just use that instead? Appreciate all the feedback and guidance thus far.

    The TPS25751 is the same package but the TPS25751 is intended for SPR (20V) while the TPS26750 is intended for EPR (48V).  If you use the TPS25751 because the EPR is not needed then the TPS4S480 is also not needed.  You can look to the TPS25751EVM as an example which replaces the TPD4S480 with the TPD4S201.

    https://www.ti.com/lit/pdf/SLVUCP9

    Regards,
    Chris

  • Hello Merri,

    Try this link for the FAQ on the input and output capacitors:  [FAQ] BQ2575X: Input And Output Capacitors 

    I can't find any other easy ways to reduce cost on your schematic

    We also have reference designs for USB charging with the BQ25756 and TPS25751 that may help:

    https://www.ti.com/tool/PMP41062

    https://www.ti.com/tool/PMP41115

    Let me know if you have any other questions.

    Best Regards,
    Ethan Galloway