Part Number: LM5180-Q1
Attached is the figure. The parameters I used are as follows:
Vin=12V, Ruv1=147K, Ruv2=34K, Rfb=130K, Rtc=360K, Rset=12K, SS pin to ground capacitance 47n, transformer ratio 1:1.33:0.5, primary winding L=26u. After the transformer are the normal rectifier circuit and filter circuit, but the test results show that the two secondary voltage outputs are 0. What's going on? Where should I start investigating?
Thanks !