Part Number: LP87524Q1EVM
Other Parts Discussed in Thread: LP87524B-Q1, AWR1642BOOST
The first issue is about the power chip not generating output voltage immediately after being powered on for a short period of time.I myself designed a test board based on AWR1642BOOST.Bought the LP87524BQ1 chip.The LP87524B-Q1 has four output channels. After powering on this chip, I detected that the voltages of SW_B0 and other four output channels were normal. However, after a short period of power-on, the four power supply pins VIN_B0, VIN_B1, VIN_B2, and VIN_B3 were pulled down to 0V, and no output voltage was detected. SW_B0, SW_B1, SW_B2, and SW_B3 all output 0V.May I ask what the reason is for this?
The second issue is that the power chip does not output voltage after being powered on for a short period of time. The second issue is that I am unable to read the register configuration of LP87524B-Q1 because there is no response.At first, I thought it was due to the lack of programming of the chip. But when I checked the forum, I found that the power supply chip was set to default values. I have an AWR1642BOOST here. I wanted to read the register-related configurations through the IIC interface, but I found that the LP87524BQ1 did not respond. The slave address I sent was 0X60.