Part Number: TPS51200A-Q1
I wish to verify whether there is a problem with the circuit diagram.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Woohyun,
Thank you for reaching out on E2E. I will review the schematic and provide my feedback before end of Friday. Thank you for your patience.
Sathish
Hi Woohyun,
Schematic looks good, except the cap at VIN pin must be increased to 4.7uF.
Sathish
Hi Sathish Vallamkonda
Thank you for reviewing the circuit.
The PCB was manufactured with a 1μF 0603 (mm) capacitor. Would changing it to 1μF cause any operational issues?
As there is no 0603 (mm) 4.7μF option in the AEC-Q specification, we would request a re-review should this be changed during PCB modification.
Hi Woohyun,
does this work for your application?
https://www.digikey.com/en/products/detail/murata-electronics/GRT188C71C475KE13D/13996898
Sathish
Hi
This is identical to the specifications you shared.
C39 1UF -> 4.7UF (https://product.samsungsem.com/mlcc/CL10Y475KO96PN.do)
Regarding your additional enquiry, could you please inform us what issues arise when applying 1UF(C39)?
Hi Woohyun,
sure, you can use an identical capacitor of your choice.
The main purpose of the input capacitor is to stabilize the input supply voltage. If the supply is not clean it may suffer from poor performance in transient load conidtions.
Sathish