REF3112: Request for Circuit Diagram Review

Part Number: REF3112
Other Parts Discussed in Thread: REF30E, REF31-Q1

 

We wish to verify whether there are any issues with the circuit diagram.

image.png

  • Hello,

    I would recommend to pay close attention to the load capacitor selection. The REF31xx-Q1 does not require a load capacitor. If a load capacitor is used, it is recommended to use one with an ESR of at least 0.5Ω. (see section 8.1 of the datasheet). For the bypass capacitor on the input, I would recommend 0.47µF (see section 8.3 of the datasheet)

    I would recommend using our new device, REF30E, which is a drop in replacement with performance improvements when compared to REF31. Please find information here:

    https://www.ti.com/product/REF30E 

    Full part number: REF3012EAIDBZR

    Thanks,

    Jackson

  • HI

    Reviewing C135 OPNE.

    If using the C135 10UF, I have an enquiry.
    Must the resistance value be at least 0.5 ohms between 0.1Hz and 10Hz?
    The capacitor in use is the GCM155D70E106M. It has no resistance value below 100Hz, but appears to be at least 1 ohm. Does it meet the recommended specifications?

    pim.murata.com/.../

  • Hello, 

    I would make sure to also take a look at the resistance up to 1 kHz to account for capacitor tolerances and variance. The ESR of GCM155D70E106M does seem to be getting a little low around that frequency. You might be fine depending on the resistance of the PCB trace, but just being cautious, I would suggest either considering a capacitor with a slightly higher ESR or adding a resistor in series with GCM155D70E106M. 

    Thanks,

    Jackson

  • Hello
    Thank you for your feedback.
    What is the difference between having the C135 (10UF) and not having it?

  • Hello,

    The output behavior for REF31 when it comes to power on and transients varies depending on the output capacitor. Pages 8-9 of the REF31-Q1 datasheet have figures which provide more detail.

    Additionally, some ADC or DAC reference pins have capacitance requirements to also take into account. 

    Thanks,

    Jackson