LM2776: Regarding <10mV ripple negative supplies for precision signal conditioning.

Part Number: LM2776
Other Parts Discussed in Thread: TPS7A30, TPS63700, TPS60402,

Hello TI support,

We are amplifying 2mV signal with precision signal conditioning circuit having gain of around=500. We need negtive supplies for the opamps. I came across LM2776 but simulation results of LM2776 show ripple of ~100mV at 20KHz with load of 5mA at -5V. Now 5mA is expected load of negative supplies in our board. 100mV will degrade the output due to PSRR, so is there a better way with TI to generate  inverted supplies with ~10mV ripple & ~5mA load current? We have +5V available in our board.

Regards,

JK