TPS7H1111-SEP: TPS7H1111-SEP's R_ref

Part Number: TPS7H1111-SEP

Would it be acceptable to set R_ref of TPS7H1111-SEP to 12.1kOhm?

The datasheet specifies 12.0 kOhm however, for internal reasons on our side, it would be preferable if 12.1 kOhm could be used. Would this be acceptable?

  • Hi Takeshi,

    Using a 12.1kOhm wouldn't cause any damage to the part but it would affect the accuracy of the part features. Section 8.3.2 provides the information on how the R_Ref pin and resistor affects the part. Below is part of the description from the section about R_REF:

    If high and precise accuracy for the part is not a high priority, using 12.1k instead of 12.0k Ohms will be okay as it's the same as using a 12k with about a 1% tolerance.

    Thanks,
    Elizabeth

  • Thank you for your reply.

    What is "accuracy"? 

    Does that mean the output voltage might differ from the design value?

    Or will the ripple increase?

  • Hi Takeshi,

    The output voltage might differ a little, but depending on your needs, the voltage output may still be within tolerance. R_REF sets the current output on the SS_SET pin which is used to set the output voltage. Changing R_REF from 12k to 12.1k Ohms will cause the reference current on SS_SET to not be 100uA. 

    Let me know if you have any more questions.
    Thanks,
    Elizabeth