This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TPS546E25: FAQ Which version of FUSION GUI supports TPS546E25 and where to get it?

Part Number: TPS546E25

 

Which version of FUSION GUI supports TPS546E25 and where to get  it? 

 

TI FUSION Digital Power Designer 7.10.5 and later supports TPS546E25

 

Version 7.10.17  is available here  Link to Product Folder

note on versions 7.10.8 to 7.10.16, the export function of programmer script is not working correctly, these versions do not include the write commands and only includes the comments. 

Go to TPS546E25 Folder 

Click Design tools

Click download options for TPS546E25-DESIGN file