I'm a little stumped here. I purchased several LP2989IMM-3.3 regulators. I'm using the 10uF Input and 4.7uFOutput ceramic capacitance values and the actual circuit is right out of the data sheet.
I get a very stable 5.01 volts out of the part on the proto-boards. It is supposed to be 3.3 volts.
I thought I had received the wrong part, but the top marking says LA2B, which seems to be correct for a 3.3 volt part.
It is the only regulator on the board, and should actually be tasked to provide 140mA at 3.3V from a 7.4V battery supply.
The only difference I can see between my circuit and the typical application circuit in the spec sheet is that I have a protection diode between input and output lines.
What am I missing?