Part Number: UCC21710
Other Parts Discussed in Thread: AMC1302
Hi...
We're planning to use UCC21710 in our application. We're getting the supply from UCC14141 to get a 15V & -4V for the gate driver. We have a 15V supply, that we're planning to as input to UCC14141.
Now, the requirement is to have an isolated 3V3 supply.
Can we take the output of UCC14141 (15V) & generate the 3V3 through an LDO ?
If so, need to understand on the GND to be considered.
As the UCC14141 is preferred for floating GNDs to drive the H-bridges, we need further clarity.
Kindly guide us in this regard.
Best Regards,
Prahaladh S