Part Number: TPS737
While testing the IC TPS73701DRVR at 48 C for 18 days We observed that the output voltage of the REG is dropped from 2.9 to 1.8V on the 18th day. We tried changing the feedback parts but the issue remains. The problem solved when we changed the IC with a new one. Details are given below.
Endurance Test 48 C - 18 Days
Desired Output Voltage - 2.9 V
Actual output Voltage - 1.8 V