Part Number: ULN2003A
Hi team,
Our customer is conducting electrostatic discharge (ESD) testing on the ULN2003A. During this testing, a failure of the ULN2003A has been observed.
Load: Relay
Phenomenon: When ESD is applied, the electrostatic discharge enters via the OUT pin, resulting in device failure.
We assume that the surge is entering through the path from OUT to COM (this is presumed to be the phenomenon described in Section 8.4, Power Supply Recommendations, of the datasheet).
When a 1 µF ceramic capacitor was added between COM and GND, the failure no longer occurred.
Questions:
- Is there any issue from a circuit standpoint with adding a ceramic capacitor between COM and GND?
- Although we do not recognize that the power supply is being applied to COM as described in Section 8.4, could you please advise if there are any recommended countermeasures?
Best regards,
Kyohei