This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61094: Question about equation 1 and 4 in TPS61094 datasheet.

Part Number: TPS61094

Hello guys,

One of my customers is considering using TPS61094 for their new product.

At this moment, they have the following question.
Could you please give me your reply?

Q.
Equation 1 on page 13, IOUT(CL)=(1-D)*(ILIM+1/2*delta IL(p-p)) 
and 4 on page 22, IOUT(MAX)=VIN*(ILIM-ILH/2*Ita)/VOUT in TPS61094 datasheet, 
they think that both of these two equations are trying to calculate the maximum current.

But these portion, "ILIM+1/2*delta IL(p-p)" and "ILIM-ILH/2" are different regardig "+" and "-".

They think that "ILIM-ILH/2" should be "ILIM+ILH/2".

Is their though correct?

Your reply would be much appreciated.

Best regards,
Kazuya.