Hi,
We are using the 3 pin LP2950 3.3V part in our system running from 24V DC supply. The intent is to generate 3.3V and use this to power the logic on the board.
I have used 10uF ceramic cap on the input side and 10uF ceramic cap with 2 Ohm resistor is series on the output side. We are seeing a output of around 5.42V from LP2950 which is unexpected. Is there anything that you could suggest to debug this behavior? Is the cap selection okay?
Best Regards,
Sridhar