I have a three cell pack using the BQ2084 fuel gauge and BQ29312 AFE with no pre charge FET. There seems to be a fundamental contradiction in the operation of CHG-FET. Any time charge termination is indicated CHG-FET turns off. But the data sheet also indicates that Fast Charge Terminate includes a followup maintenance charge. Indeed the fuel gauge will ask for maintenance current from the level 2 charger while it has also commanded CHG-FET off resulting in no charging current flowing to the cells. There is a CHGFET bit setting in misc. config. data flash that can keep CHG-FET on in charge termination. When this is setup this way all charge current commanded by the fuel gauge (including 0mA requests) are properly delivered and charging appears normal.
Why does BQ2084 turn off CHG-FET when it is also asking for current from the level 2 charger? Why is the CHGFET option provided? What is the downside to keeping the CHGFET on in charge termination? Is turning off CHG-FET under charge termination indication the intended way to shut off the charging current instead of commanding the level 2 charger? When a level 2 charger is in use should CHGFET always be set to keep CHG-FET on in charge termination?