Hi!
Please find the attached PDF for the implemented TPS63002 design.
The EN_USB signal is coming from the uc (An MSP430)
When the IC is disabled, it is not heating up. But when enabled it heats up, even though no load is connected to it.
When checked on oscilloscope the 5 V Waveform is seen, though it is still a little choppy.
Initially the powerpad was not connected to ground, but it is now connected to ground.
The source of power is Li-Ion battery. Is it necessary to PS/SYNC to ground if using a Li-Ion battery?
Could this be because of the selection of inductor and capacitor?
Looking forward for assistance.
Kind Regards,
Aditya Ayachit