I need to use some TI components in my circuit for the competition I am in. I would like to use something like the MCP73831 (http://www.sparkfun.com/datasheets/Prototyping/Batteries/MCP73831T.pdf) because in my application I need as small a footprint as possible, so the fewer extra components the better. I'm trying to charge a single Li-ION or Li-Pol battery with 120 mAh capacity, so the low charge current is important. I'd looked at the BQ24203, but it provides a minimum charge current of 400 mA, so that won't work. I need more like 100 mA.
If anyone knows of a good TI chip i can use, let me know. Thanks!