Hi specialists
I ask myselfe if I can use the integrated DC/DC power module TPS84620 as a LED driver for constant current. The idea is to use either the Vadj input or the Sense+ input as a feedback comming from a sense resistor in series to the LED load. The output voltage will be set for 2.9V with Rset and increase by the parallel FET immediatelly after switch on. The current feedback will close the FET and reduce the output voltage. The current set should be the reference voltage divided by the LED sense resistor.
Could the reference voltage made by a Schottky diode if the accuracy of the current is not so important ?
Thanks for your advices. regards N.