This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTN78000AAH Maximum Output Current and Temperature Derating

Other Parts Discussed in Thread: PTN78060A

Our product uses a PTN78000AAH voltage regulator module with a 24V input and a -15V output.  I have discovered that the regulator is supplying approximately 0.75A continuously.  The datasheet maximum output current is 0.6A at -15V with an ambient temperature of 85°C with natural convection airflow.

Our product's upper ambient temperature specification for the equipment is 49°C.  Let's assume that the ambient temperature of the regulator is somewhat higher at 55°C in the case with natural convection airflow.  If I extrapolate the temperature derating vs. output current curve for a 12V input (the 24V input curve isn't given in the datasheet for a -15V output) it is approximately 0.75A at 55°C.  I know that this doesn't give much margin, but can I interpret the curve this way, or will this lead to potential early failures?  If so, is there the curve available for a 24V input a -15V output?

I could upgrade to the PTN78060A, but it is not footprint compatible and would require a board spin.  For you information we are using 2 oz. copper.

I appreciate any feedback.

Thanks,

Dom Megran

  • PTN78000AAH maximum input voltage with (-)15Vout is +17V. ThePTN78XXXAXX  Modules absolute maximum Vin is =17V with Vout (-) 15V. Buck boost absolute voltage  Vin+Vout=32V. The PTN must not be used with 24Vin. The PTN78000AAH maximum output current (-15VOut) is limited to 600mA with either (+) 12Vin or (+)15Vin.

    There are several alternative power solutions fo (-)15Vout at 750mA.  

    Convert +24V to either +12V or +15V with a   step down regulator.

    1. PTH78000HAx can be used to down convert  from + 24V in to +15Vout .Maximum ambient temperatures  with no  air flow  WITH 1A output current is 80°C

    1. Add a front  power device with input of (+)24V and output of (+)15V. Then connect (+)15V to the  PTN78060AAx input  voltage pin. The output voltage can be adjusted to (-) 15V at 750mA.

    a. The PTN78060AAx thermal section(SOA) of the data  sheet  with no air flow at (-)15V Vout with 12V or 15Vin has a +70°C maximum ambient temperature with no air flow.

    Tom