This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCV010515D Output Power

Other Parts Discussed in Thread: DCV010515D

Hello,

My question is if the 1W output of DCV010515D is limited in 0,5W to each output (+15V or -15V) or shared in any proportion (P@15V [0,8W] + P@-15V [0,2W] = 1W) ?

Regards,

Mateus.

  • DCV010515D  each polarity can share  total output power of 1W.The output voltage will be slightly lower on the higher current bus .The output capacitors are to be ceramic types which should be  2.2uF or greater  for better attenuation of the  output ripple.

    Tom