Hello,
Can the LMZ10500 and LMZ10501 work in a negative inverter topology? If so, can you provide an application note or reference design. Thank you. I'm interested in getting a -5V, -3.3V, and -1.2V output from a positive 5V input.
David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Can the LMZ10500 and LMZ10501 work in a negative inverter topology? If so, can you provide an application note or reference design. Thank you. I'm interested in getting a -5V, -3.3V, and -1.2V output from a positive 5V input.
David
Hi David,
Yes the LMZ10500 and LMZ10501 can be used in an inverting topology but of the voltages you are looking at would only work for 3.3Vin to -1.2Vout.
For the -3.3V and -5V you could use the LMR14206, which is a very compact design. Or if you want to stay with a module the LMZ12003.
In terms of an application note, I will point you to a post, where I discuss the inverting application in more detail
and here is an application note with more information on inverting designs.
http://www.ti.com/lit/an/slva317a/slva317a.pdf
Regards,
Marc
I am also interested in generating negative supply with this type of parts but the links do not work here.
Where could i find more?
The name of an ap note for the LMz14203 is.
The link for that ap-note is