I am using it to power a FPGA PLL input voltage of 1.8V at 11mA.
This FPGA input voltage has a requirement of no larger than 10mV pp ripple up to 80MHz. I am wondering if the LM4132 can meet this requirement. I have a feeling it will, but I can only see the output noise voltage only spec to 10Hz, which is much lower frequency range than I need. Thanks.