Hello
Has anyone tried breadboarding the TPS63061? If so , does anybody have any tips ? I'm trying to build a circuit that will provide a 5 Volt output with either a 12 V or a 3.7 V input. Your help is highly appreciated.
Sankalp Prakash
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
Has anyone tried breadboarding the TPS63061? If so , does anybody have any tips ? I'm trying to build a circuit that will provide a 5 Volt output with either a 12 V or a 3.7 V input. Your help is highly appreciated.
Sankalp Prakash
Our switch-mode power supplies are best evaluated on their respective evaluation modules.
The TPS65061 can be evaluated on the TPS63060EVM-619.
A bread board adds too much impedence for the switcher to operate properly.
Also note the SON10 package will not be compatible with a DIP breadboard.