Other Parts Discussed in Thread: BQ76925, BQ77910A
A couple questions...
In a bq76925, is there any appreciable delay or processing time before VIOUT follows any changes in charge/discharge current levels? Other than the time that Cout would take to charge/discharge and the acquisition time by the microcontroller, that is. We have an application that would require polling the ADC measuring VIOUT at least 10x/second and we're hoping that VIOUT updates almost immediately.
We'd also like to test the bq76925 in an application requiring disconnecting/reconnecting of the battery pack (4S LiFePO4) via a single connector. Assuming that VBAT and each VCx pin is protected by a properly spec'd zener to VSS or VC0, do you recommend also adding pin-to-pin protection between VC0+VC1, VC1+VC2, etc., via an 8.2V zener (max = 8.45V) for each? Or would this interfere with use of on-board balancing and open-cell detection?
Thank you!