This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63061 Vout regulation with Vin = 14V

Other Parts Discussed in Thread: TPS63061, TPS54240

I know that the absolute maximum rating for Vin on the TPS63061 is 17 Volts. My application requires a 14 Volt input to the TPS chip. The device that I plan to connect to the TPS63061 5 Volt output draws 2.2 Amps.  The datasheet calls for a Vin of 2.5 to 12 Volt. Will the TPS63061 be able to provide a regulated output voltage of 5 volts even with a 14 Volt Vin?

Thanks

Sankalp Prakash