In the bq20Z655-R1 release we have noted a preemption of the broadcast capability with the BCAST bit set (Operation Cfg B, Low Byte, Bit 0 = 1) when the SBS 1.1 Master Mode Bus Start Collisiton Update feature is enabled (default settings). The default setting for SMB Sync Command is 0xff (any command) with an SMB Sync Delay of 50 (50 X 488uS = 24.4mS). The intent of this feature is to delay the mastering of the SM bus by the gas gauge after it has received an SMB command to reduce the likelihood of collisions. However, unless the feature is deactivated (SMB Sync Delay = 0), we have observed that no periodic (~50 sec) broadcast messages for ChargingVoltage() and ChargingCurrent() occur when the SMB signals are pulled up by a charger or host, and alarm messages appear to be inhibited as well. Have others observed this behavior? Solutions?