I'm using a bq27200 gauge in a system with a typical load of 500mA; I've selected EDV1 for the C/16 point as per the programming instructions. On occasion the load can be as high as 1.5A, when this occurs EDV1 is reached well before C/16. When this happens during a qualified learning discharge, the gauge re-calibrates to a falsely low C.
Has this issue been encountered by other users? Is there a way to prevent this erroneous calibration from occurring?
Any help/advice will be appreciated.