This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSP65910 RTC not running

Other Parts Discussed in Thread: AM3715, TPS65910

RTC_CTRL_REG STOP bit is never being set.

What things should I be checking for?

I'm using linux derived software for the AM3715. I set the CTRL STOP bit and check the STATUS run bit and that's not set. When I re-read the CTRL STOP bit it is not set.

My 32kHz crystal is running OK. My main board is up and running fine - the RTC is one of the last jobs to do. I have done test write  and read to the BACKUP Register and that checks out so I think my i2c comms are OK.

Any hints?

(I don't think there is an MSECURE bit on this device so I don't have to worry about that I hope.)