Hello,
is it possible to connect two or more LMZ14203(H) in parallel to get a higher output current?
Best Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
It should not be a problem to use one resistor divider for both ICs.
The RMS-current will not be higher than 3A. But I have to handle current peaks of 6A.
So only IC would be capable to handle the average power.
Are there any other problem, rather than current sharing, which have to be considered?
Hello there,
Unfortunately the 3A modules (LMZ1420x/xH) are not designed for current sharing. Consider the 6Amp LMZ23606H or the 8 Amp LMZ23608 (scheduled for release in September)
Both of these are rated for 26V max input voltage and up to 15V output level. They also happen to support current sharing. Small quantity samples are available now.
Alan Martin TI-SVA
Hello,
is it possible to get some early samples of the LMZ23608h?
I would need at least 2. If they are not available the LMZ23606H
would be the second choice. I can not find them anywhere on the web site.
Best regards
Markus Erber
Hi Markus,
These products are not available quite yet. They will release in end of September. If you would like samples of the LMZ23608H, please email me at Colleen.Kilroy@ti.com with your mailing address. Thanks for your interest in the power modules!
Regards,
Colleen