Hi
I have a charger which uses the Li-ion linear charger, BQ24061. I am precisely using the application circuit on page 12 of the datasheet (Figure 16: Application Circuits, the second one which corresponds to BQ24061). I am charging the 18650 3.7V-nominal 2600-mAhr Li-ion cell. Unfortunately I designed my board such that I can flip the polarity of the 18650. I noticed that when I do that, the charger ic becomes damaged and I cannot use it anymore.
I believe the source of my problem is the high current which the BQ24061 has to carry when I flip the polarity of my battery. How can I avoid this problem. Right now I am thinking of using a pass PFET and comparator. I would like to hear some suggestions.
Thanks
Edison