So in my application I have a power source that is ideally at 3.6V but can drop as low as 2.6V while the circuity it powers needs a well regulated 3.6V. The load, however, is a pretty light typical amount of 5mA or so, though it can go up to 40mA. My question is what, in general, happens in a boost or buck-boost integrated circuit when the load current is considerably low like this? Also, what will happen in a boost converter IC in the case when the input voltage is already equal to the output voltage? For my application what would be a better topology to go with, the boost or the buck-boost?