This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCV010515D Inrush current

Other Parts Discussed in Thread: DCV010515D

Hi,

I'm using the DCV010515D in a module (board) of my system. When I use more than 4 boards, the inrush current is so high that my main power supply module can provide enough power. My power module has 6A@5V. So, when used 4 modules with DCV010515D, the inrush current is more or less 1.5 A.  How can I reduce this inrush current  ? I'm using the capacitor type and value (ceramic 2,2uF low ESR)  as mentioned in the datasheet and very close to the input pins.