This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90SEQ64EVM-650 UCD90124A JTAG clock

Other Parts Discussed in Thread: UCD90SEQ64EVM-650, UCD90124A

I recently ordered a UCD90SEQ64EVM-650 board for developing with the UCD90124A.  On the board I have, R9 and R10 were both installed.  This shorts the TCK and TRCK pins.  My cable was unable to 'overdrive' the clock pin, so the JTAG clock had a high voltage of approx. 1V.  According to the schematic here: http://www.ti.com/lit/ug/slvu423/slvu423.pdf  R10 is not supposed to be populated.  After removing R10 I was able to scan the JTAG chain correctly and the JTAG TCK pin looks as I expect.