Hello, Does the LM3480 linear regulator require input and output caps to assure stability? http://www.ti.com/lit/ds/snvs011d/snvs011d.pdf ...the datasheet does not speak of this capacitance and stability. So is the LM3480 immune to instability?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, Does the LM3480 linear regulator require input and output caps to assure stability? http://www.ti.com/lit/ds/snvs011d/snvs011d.pdf ...the datasheet does not speak of this capacitance and stability. So is the LM3480 immune to instability?
Nothing is said about stability, but all the performance characteristics are plotted with Cin = Cout = 0.1uF
Special IC design considerations have to be taken into account to allow for no input/output cap linear regulators. For min capacitance this part was most likely characterized with the circuit shown in the typical applications section (0.1uF for input and output). I would not recommend going lower than these values.
Regards,
Dennis
Hi at all.
I have another question regarding the LM3480 - and found no better place to write into! So, here's my question:
Is the LM3480 protected against reverse polarity of supply voltage? I found no information in the datasheet.
Thanks in advance,
Guido