This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1825 Clock Sync Range

Other Parts Discussed in Thread: UC1825A

Hello! RE: UC1825A, I would like to know the clock sync range given a free run freq of 450kHz and a clock sync circuit which will pull this up to 465kHz and could pull it up to 625kHz. The power stage is OK with all these frequencies. This question is what limitations are there to the clock sync range? Can the Free run freq at 465kHz be synced up to 1MHz? Do you have any concerns about doing this?

 

Thanks,

Regards,

Bill