Under Battery Switch Operation on LP3972 data sheet page 16/62, It is stated that the battery switch may be disabled when only a main battery is used by setting the “no back up battery bit” in the control register 8h’0B bit 7 NBUB.
Since switching will not occur with this bit set (i.e. the LDO_RTC will remain connected to the main battery), is that a must to connect the backup battery input (pin 15) to main battery input (pin 6) as stated in the data sheet?
Kindly enlighten what is the side effect if this backup battery input pin is left floating / unconnected (with NBUB bit set to 1)?
Regards
Cheok