I am looking for a Half bridge gate driver with the following specs.
-Operate at 28VDC.
-Output 500mA
-Can be configured as high impedance.
-Switching speed less then 200ns.
I found the LM5105 that will meet these specs, but I have a few questions about this IC.
1. Will the LM5105 operate at DC (0Hz) if I provide a power source to keep the high side gate driver bootstrap capacitor charged?
2. Will a charge pump work to generate a high voltage (maybe 45V) along with a current limiter and zener diode across the bootstrap capacitor in order to prevent the bootstrap capacitor from discharging during DC operation?
Any feedback would be much appreciated. Thanks for the help.