This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54494 LDO Output

Other Parts Discussed in Thread: TPS54494

Hello,

From TPS54494  Datasheet (TPS54494 SLVSBH1 –JUNE 2012) page 5

REF1. ""VREG5: Output of 5.5V linear regulator. Bypass to GND with a high-quality ceramic capacitor of at least
1.0 µF. VREG5 is active when ENx is high.""

REF2. Funtional Block Diagram (page 6)

5VREG use VIN1 Input only. No control fro ENx pins.

I use power good PG1 (from first converter) with pull-up connected with 5VREG for control EN2 pin (second converter).

And I not sure that this will work, because according REF1 VREG5 active with BOTH ENx enabled.

So datasheet provide or wrong description or wrong diagram.

How use power good from 1-st converter for control second if LDO active when BOTH enabled?

Use external supply for PG1 pull-up? But what is purpose of VREG5 in this situation?