Hi,
I'm using a TPS61097-33 in a solar/battery powered application where my Vin may vary between 1.5V and 5V. The regulator works great for low voltages on Vin, but when Vin raises, Vout raises as well. I get a nice 3.3V output until Vin is between 1.5 and 3.5V. At 5V on Vin I have almost 4.2V on Vout. Have I missed something fundamental? I thought I should be able to go up to 5.5V and still have 3.3 on Vout? My circuit is the same as in the datasheet, having 10uF on C1 and C2 and 10uH on L1. My application consumes between 1-10mA during the tests when I experienced this.
Thank's for any info about this!
/ Mikael