This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24272

Other Parts Discussed in Thread: BQ24272

Dear Experts,

We are using in our design BQ24272 chip for charging one cell Li-Ion battery and managing the power path for the given application.

The chip it does as expected exceping one fact:

When the battery is depleted  (Vbat reached  Vbattuvlo =2.5V)-trough the external fet driven by the BGATE pin even when is off itt will a be current flowing trough the intrinsec diode of the FET

Question:

Can we overcome the above issue (avoiding depleting the battery below 2.5V) by using 2 MOSFET's P channel back to back?

If Yes, will the internal MOSFET 's diode conduct in the same manner or is in fact a back to back topology switch?

Thank you, Endre