I want to use the BQ24005 to design a charge circuit for a 2 Cell Li-ion battery: 8.4V 1200mAh.
I read in the BQ24004/5/6 user guide (SLUU110A) on page 1-2 under table 1-1 the following:
"Vi for a 2-cell, should not exceed 9.1 VDC for the 1A charge current..."
Does this mean the supply voltage on pins 2 and 3 (IN) has to be 9.1V???
What happens if the voltage is 9.0V or 9.2V???