Hello,
I am having some issues on getting my BQ24105 chip to start charging and I am wondering if anyone can assist me with this. We are using this IC to charge a 3 Cell 12.6V Battery.
The issue I am seeing is that the board we designed for the BQ24105 does not begin charging. The chip does come alive but it seems like it is stuck in the battery absent mode. The reason I believe it is stuck in this mode is because when there is no battery connected, we see the output voltage constantly jump for both our board as well as the EVM board. Once the battery is connected, the Stat1 LED on the EVM goes on, which indicates it is charging. I also notice that VIset1 and VIset2 are present on the EVM board but not on our board.
From what I am aware of, most of the layout as well as component values are identical to that of the bqSWITCHER EVM board. The only difference is the resistor values used for the TS line, which we are not currently using.
We are using a MSP430 to drive the Chip Enables and to read in the Stat1 and Stat2 pins. The only issue I can think of is that the 3.3V MSP we are using is not enough to enable and disable the chip.
Is there anything that we need to look for that will help us enable the bq24105?